שאלות נפוצות
Which M580 controllers support LL984?
Issue
An M580 controller is needed that supports 984 Ladder Logic.
Product line
Unity Pro, M580
Resolution
Only the following M580 controllers support 984 Ladder Logic programming:
BMEH584040
BMEH586040
BMEP584040
BMEP585040
BMEP586040
BMEP584040S
**minimum Unity Pro v11.0
An M580 controller is needed that supports 984 Ladder Logic.
Product line
Unity Pro, M580
Resolution
Only the following M580 controllers support 984 Ladder Logic programming:
BMEH584040
BMEH586040
BMEP584040
BMEP585040
BMEP586040
BMEP584040S
**minimum Unity Pro v11.0
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
טווח:
גלה עוד
טווח: