Can we use SF / UTP AWG24 ethernet cable for variable speed drives Altivar ATV32, 320,340, ATV630 (embedded+advanced eth, ATV930 ?
Yes, it is possible, the Ethernet cable cross-section does not need to be AWG22 min, it is enough to be AWG24 or any greater cross-section. The recommendation is to keep the SF/FTP type