המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is there a trial version of EcoStruxure Control Expert?

Article available in these languages: Spanish

Control Expert comes with a 30 day trial license.

When the first installation is complete, the trial license is automatically activated during first launch of the software.

The trial license includes the maximum set of software product features which corresponds to the
Control Expert  XL package with M580  Safety Add-On.

If you do not activate your license within 30 days, Control Expert will no longer run once the trial period has expired.