שאלות נפוצות
What to do if a message with ID 0x1480, 0x1481 or 0x1482 is displayed on the MicroLogic X screen.
These messages are generated by the Maintenance Schedule function of the MicroLogic X control unit, to indicate that a preventive maintenance operation is due.
Refer to the MicroLogic X User Guide:
Refer to the MicroLogic X User Guide:
- For information about the Maintenance Schedule function and recommended actions.
- For information about how to acknowledge a message on the MicroLogic X screen
- For information about message 0x1480 and the basic end-user preventive maintenance program.
- For information about message 0x1481, and the standard end-user preventive maintenance program.
- For information about message 0x1482, and the manufacturer preventive maintenance program.
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
טווח:
גלה עוד
טווח: