שאלות נפוצות
What to do if a message with ID 0x1445 or 0x1446 is displayed on the MicroLogic X screen.
These messages are generated by the MicroLogic X Service Life Monitoring function of the MicroLogic X control unit, to indicate that a predefined usage threshold is reached.
Refer to the MicroLogic X User Guide:
Refer to the MicroLogic X User Guide:
- For information about the MicroLogic X Service Life Monitoring function and recommended actions.
- For information about how to acknowledge a message on the MicroLogic X screen
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
טווח:
גלה עוד
טווח: