המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can I perform a product reset of an ATV320 over network control?
Issue:
Customer wants to be able to perform a product reset over the network instead of sending someone to the remote location to manually cycle power.

Product Line:
ATV320

Environment:
All

Cause:
Clarification of product capabilities.

Resolution:
Yes, this is possible.  Please see full instructions below:
We give the logic address of RP and to know the value to write, you should click on N_Y in Link column (be careful this one is R/WS - See Access column):

User-added image

You will see the definition below:

So to reset the product, you should write 1 .

User-added image


R/WS access means that the value is written only when drive is in STOP or fault ( not running). So this is a configuration parameter, which means that it should not be put on IO scanner of Ethernet or any cyclic write of any fieldbus. If you do, the drive will never start, and stay locked on NST.

So, to write RP, you should use messaging (not cyclic exchange), and be sure that the write request of RP=1 (to reset product) is sent one time , otherwise, the drive will continually reset.