The following are the power dissipation values of the METSECT5 series current transformers:
Reference number: | Power Dissipation @Icth |
METSECT5CC…. | ≤ 3 W |
METSECT5MB…. | ≤ 11,5 W |
METSECT5MA…. | ≤ 7 W |
METSECT5MC…. | ≤ 9 W |
METSECT5MD…. | ≤ 10,5 W |
METSECT5DA…. | ≤ 20 W |
METSECT5DB…. | ≤ 23 W |
METSECT5DC…. | ≤ 23 W |
METSECT5DD…. | ≤ 19 W |
METSECT5DE…. | ≤ 27 W |
METSECT5DH…. | ≤ 25 W |