שאלות נפוצות
Easy UPS Line Interactive UPSCAPO Software Download
Issue:
The customer is unable to install the Easy UPS Line Interactive UPSCAPO software from the supplied CD.
Resolution:
Download and extract the file attached below. Once extracted go into the UPSCAPO-Management Software folder and double click Setup.
Follow the on screen instructions to complete the installation.
The customer is unable to install the Easy UPS Line Interactive UPSCAPO software from the supplied CD.
Resolution:
Download and extract the file attached below. Once extracted go into the UPSCAPO-Management Software folder and double click Setup.
Follow the on screen instructions to complete the installation.
פורסם עבור:שניידר אלקטריק ישראל
קבצים מצורפים
גלה עוד
טווח:
גלה עוד
טווח: