{}

המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
What are the new features in Link150 firmware version v5.1.15
Product Line
Link150 (EGX150)

Environment
Release Notes

Resolution
While the attached document has the complete information, here are the new features in this firmware version:

•    Security updates in support of:
o    Internal cyber security initiative
o    Self-signed certificate for 38 years
o    Link150 device in "HTTPS enabled" mode by default
o    RBAC-User Account Management supported with Admin and Guest pre-defined roles

•    Enhancements:
o    New Web page UI layout
o    RSTP feature supported
o    Firmware upgrade through web page supported for versions for 5.1.15

•    Other updates:
o    FTP feature removed for better security improvement.
o    Web page access (Admin and Guest) are with pre-defined roles.
o    Firmware 5.1.15 version is not backward compatible with existing User Account Management. By upgrading to firmware version 5.1.15, user will lose all the user account settings.
o    User guide is updated for web navigation and other features for firmware version 5.1.15. Refer to Chapter 3.
o    Connection of Modbus TCP/IP is not configurable from firmware version 5.1.15 and supports up to 32 address.
o    Link150 device with firmware version 5.1.15 cannot be downgraded to older version of firmware (up to version 5.0.29).
Link150 firmware can be downloaded from here .

שניידר אלקטריק ישראל

קבצים מצורפים
Link150_Release_Notes.pdf [402.15 KB]
גלה עוד
טווח:
מאמרים שעשויים להיות מועילים
גלה עוד
טווח: