שאלות נפוצות
Can we reuse screws for connections of MasterPact Air Circuit Breakers?
This applies to MasterPact ACB's including:
MTZ
NW
NT
The screws used to reinforce the connection to the MasterPact line can be reused on the same unit if they are not damaged (according to visual inspection).
![Connections of MasterPact Air Circuit Breakers](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000D8thnQAB&oid=00DA0000000abSmMAI)
68570366
MTZ
NW
NT
The screws used to reinforce the connection to the MasterPact line can be reused on the same unit if they are not damaged (according to visual inspection).
68570366
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
טווח:
גלה עוד
טווח: