Issue
Manual control actions include actions such as resetting values on devices or changing device configuration settings. You can also set the confirmation method that is used by the software to confirm a control action request before carrying it out.
Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
Vista
Web Application
Resolution
*Warning: Do not use the software to control time-critical functions. Do not use the software to control remote equipment without proper access control and status feedback.*
You can enable or disable the ability to perform manual control actions in Diagrams. Manual control actions include actions such as resetting values on devices or changing device configuration settings. You can also set the confirmation method that is used by the software to confirm a control action request before carrying it out.
Control in Diagrams is disabled by default.
NOTE: The required user access permissions for performing a control action are configured individually for each control object in a diagram. This is done at design time in Vista. However, to perform any control action in Diagrams you need at least controller-level access or higher (operator-level, supervisor-level). This is true even if the permissions for a control object in a diagram are set to user-level or view-only-level. Only through Vista can users with user-level or view-only-level access perform control actions on such a control object. To view or change the permissions on a control object, open the diagram in Vista.
NOTE: Control in Diagrams is only available when an HTTPS connection is used between the PME server and the Web Applications client.
To enable or disable control in Diagrams:
- Open the Settings page from the SETTINGS link in the Web Applications banner.
- In the Settings Library select Security > Diagrams Control Options.
- In Diagrams Control Options, enable or disable manual control in Diagrams.
- Click Save.
To set the confirmation method:
NOTE: Control in Diagrams must be enabled for the confirmation method settings to be displayed.
- Open the Settings page from the SETTINGS link in the Web Applications banner.
- In the Settings Library select Security > Diagrams Control Options.
- In Diagrams Control Options, select the confirmation method - Dialog Box without Password or Dialog Box with Password.
- Click Save.
פורסם עבור:שניידר אלקטריק ישראל