שאלות נפוצות
Is the Vijeo Designer project file .vdz included in the file system download files ?
Issue:
Vijeo Designer project file .vdz included in the file system download files
Product Line:
Vijeo Designer
Resolution:
The only way the vdz file would be included in the File system download files, is if the "include editor project" option was enabled in the project. If this is the case, the vdz file is located in the following path PUBLIC\PROJECTS\TARGET1\DATA\PROJECT. TARGET1 folder is the default name for the target, this could be a different name. If the vdz file is not located in this path, then the "include editor project" option was enabled in the project and therefore the vdz file would not be included.
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
טווח:
גלה עוד
טווח: