שאלות נפוצות
Is Daylight Savings Time (DST) configurable in a Momentum processor?
Daylight Savings Time (DST) is not configurable in a Momentum PLC. Although the 'TIME' configuration screen in Control Expert V15 (and lower), Tools > Project Settings, allows the user to make changes, it is not applicable for this product. This setting is scheduled to be disabled for the affected processors in Control Expert 15.1.
DST can be implemented to change automatically through user code.
The products affect are:
171CBU98090
171CBU98091
171CBU78090
DST can be implemented to change automatically through user code.
The products affect are:
171CBU98090
171CBU98091
171CBU78090
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
מוצר:
גלה עוד
מוצר: