{}

המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
In Ecodial 4.9.4FR ,What is the application of Micrologic 2.2AB and Micrologic 4.2AB
In France , MicroLogic AB trip units are used in public distribution systems to limit the current supplied according to the consumer's contract. They are available in 100, 160, 240 and 400 A ratings and are supplied with a lead-seal device to protect the settings.

שניידר אלקטריק ישראל

In Ecodial 4.9.4FR ,What is the application of Micrologic 2.2AB and Micrologic 4.2AB
In France , MicroLogic AB trip units are used in public distribution systems to limit the current supplied according to the consumer's contract. They are available in 100, 160, 240 and 400 A ratings and are supplied with a lead-seal device to protect the settings.