{}

המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
What are the features available in TeSys Giga advanced type contactors ?
Along with direct coil control, advanced type contactors have PLC input control option. And it’s always installed with cable memory kit for an easy and quick maintenance. It has comparatively lower coil consumption and it's also ready for connectivity to EcoStruxure (via PLC control to EcoStruxure architecture). The advanced version can be installed with a Remote Wear Diagnosis (RWD) module, for remote signalling and control purposes.