שאלות נפוצות
Does Facility Expert retrieve the entire bill of material when a project is exported from EPC to FE ?
Yes, Facility Expert will retrieve all the information from EcoStruxure Power commission tool (Switchboards, all assets hierarchy under the switchboard, test reports, any other documents attached in EPC ),no matter how the devices are added in EPC (auto discovery or QR code scan),
Attention : If devices are added through QR code scan in EPC, these devices will be categorized as "Electrical Equipment - Others - Others" when they land on Facility Expert.
Attention : If devices are added through QR code scan in EPC, these devices will be categorized as "Electrical Equipment - Others - Others" when they land on Facility Expert.
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
מוצר:
גלה עוד
מוצר: