{}

המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
Can the coil/control module on the same rating of Giga contactors be changed to a different voltage control module in the field ?
No, we don’t recommend customer to change the control module to a different voltage in the field, it will lead on-site confusion for all marking vs. real product.

Note: Control module spare parts are available and can be replaced in less than 10 minutes

שניידר אלקטריק ישראל

Can the coil/control module on the same rating of Giga contactors be changed to a different voltage control module in the field ?
No, we don’t recommend customer to change the control module to a different voltage in the field, it will lead on-site confusion for all marking vs. real product.

Note: Control module spare parts are available and can be replaced in less than 10 minutes