שאלות נפוצות
Do the HMISTM6200 and HMISTM6400 include the front screen and back unit?
Issue:
Do the HMISTM6200 and HMISTM6400 include the front screen and back unit?
Product Line:
Modular Harmony STM6.
Resolution:
The HMI Modular panel HMISTM6200 is a combination of a display module 4” (HMISTM62) and a rear module (HMISTM6B) that are mounted through a 22mm hole.
The HMI Modular panel HMISTM6400 is a combination of a display module 4” (HMISTM64) and a rear module (HMISTM6B) that are mounted through a 22mm hole.
See the Harmony ST6 High-resolution and cost-efficient basic HMI Catalog available here:
https://download.schneider-electric.com/files?p_enDocType=Catalog&p_File_Name=Harmony+ST6+High-resolution+and+cost-efficient+basic+HMI+Catalog.pdf&p_Doc_Ref=DIA5ED2181202EN
NOTE: To program these HMI models, use the EcoStruxure Operator Terminal Expert software.
https://www.se.com/ww/en/product-range/62621-ecostruxure-operator-terminal-expert/
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)