Issue:
Character "œ" appears incorrectly during Runtime
Product Line:
EcoStruxure Operator Terminal Expert, Harmony HMI,
Resolution:
The language fonts on EcoStruxure Operator Terminal Expert are regulated by ISO standards.
The French_Gothic font set uses the character code [ISO IEC8859-1]. The "œ" character can not be displayed because it is a character that does not exist in the [ISO IEC 8859-1] character code.
Instead, use the Romanian_Gothic font set. This uses the character code [ISO IEC8859-16] which includes the "œ" character.
פורסם עבור:שניידר אלקטריק ישראל