{}

המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
How to read the last Event inside an IED device (IEC61850) buffer report from a BMENOP0300 after an M580 swap?
Context:
In some architecture IEC61850 where M580 HSBY and BMENOP0300 are used, BMENOP0300 is used as client function and communicate with IED device (Protection Relay for example) by using Buffer report.
The buffer report inside the IED device is read by the BMENOP0300.
When using Report Functions, it is recommended to automatically enable the report function for buffered and unbuffered report control blocks by setting the “AutoEna” field to 1 (auto enable). After switchover, the BMENOP0300 module will automatically enables the report when establishing a connection with the remote IED.

IEC61850 configuration device ddt

However, by using Buffer report, during a switchover, the new primary rack will enable the report and read all the events contain in the IED device buffer. For example, inside the IED buffer if there are 50 events, the NOP will read all those 50 events and will make a change from 0 – 1 – 0 – 1 …. 50 times.

Therefore, when using buffer report in a M580 HSBY, we recommend to not set the “AutoEna” field to 1 and to follow the step below in order to read the last event entry inside the buffer (by using the EntryID attribute) before enabling the report:

Auto Enable should be always at 0
IEC61850 configuration device ddt

After a Swap, the report will not be enable. The following step need to be performed and automatize :
Check Health bit with IED

IEC61850 configuration device ddt

Need to read EntryIDs with option “108”

IEC61850 configuration device ddt

Give a Trigger on the “cmd”
You can see that the IED device replied with the number of EntryIDs
IEC61850 configuration device ddt

Write EntryIDs with option “8” to the IED Device
IEC61850 configuration device ddt

Give a Trigger on the “cmd”
IEC61850 configuration device ddt
You can see that the “write” has been well sent because the Report Status give “OK”

Form this point we can proceed to enable report :
Make sure attribute is “1”
Enable Report with option “1”
IEC61850 configuration device ddt

Give a Trigger on the “cmd”
IEC61850 configuration device ddt

At this point, the BMENOP0300 has received only the last event from the buffer of the IED device and report is enable.


Product line
BMENOP0300, M580 HSBY

Environment
Windows, IED device, buffer report

שניידר אלקטריק ישראל

גלה עוד
מוצר:
מאמרים שעשויים להיות מועילים
גלה עוד
מוצר: