{}

המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
Scadapack Workbench Installation issue, Installed OPC Foundation DA 3.0 redistributable version too old.
When installing SCADAPack Workbench, a warning message may appear "Installed OPC Foundation DA 3.0 redistributable version is too old."

OPC_SW
  • A potential solution is try to reinstall the OPC Core Components Redistributable (x86) manually. The OPC Core Components Redistributable (x86) installation software can be found in the 
    Scadapack Workbench installation software. SCADAPack Workbench and Utilities 6.6.8a\SCADAPack Workbench\Prerequisites\OPC Core Components\x86
If this does not help, please get in touch with your local support team for further assistance.