Issue:
Can I monitor 2 or more External Battery packs Temperature Sensor for SRTG15KVA and SRTG20KVA?
Product Line:
SRTG15KXLI,SRTG20KXLI
Environment:
All models, All Serial Numbers
Answer:
No! only 1 at a time are able to monitor or attached to the UPS.
Some customers may attempt to monitor 2 or more external battery pack temperature sensor but the default is not. They can only attached or monitor a single external battery pack temperature sensor.
Actual connection:
See image below:
פורסם עבור:שניידר אלקטריק ישראל