undefined undefined
{}

המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
Automatically Acknowledge Orange pop up messages on the Micrologic X Display
Issue: I have a high inrush current application like a motor starting and the long time start or short time start Orange alarm pop up message keeps coming on.  How do I auto acknowledge those alarms?

Product Line: Masterpact MTZ Micrologic X Control unit

Environment: Micrologic X Firmware Version 004.107.000 and above

Resolution:
If you want to automatically acknowledge Orange Alarm pop up messages on the Micrologic X display such as long time Ir start or short time Isd start, use the auto acknowledge feature available in Firmware Version 004.107.000 and above.

Example Orange alarm pop up message:
Orange alarmIr start alarm

Micrologic X Firmware release notes:
FW release notes


HMI Configuration of Auto Acknowledge:
HMI configuration 1
HMI configuration 2