undefined [object Object]
{}

המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
PowerChute Network Shutdown ESXi host shutdown failed for vSAN standard cluster with Skip Maintenance mode enabled.
Issue:
 ESXi host PowerChute Network Shutdown is running on failure to shutdown when configured for vSAN, and enabling Skip Maintenance mode has been selected.

Product:
PowerChute Network Shutdown version 5.x

Environment:
PowerChute deployed onto a vSAN datastore.
VMWare ESXi 7.x or 8.x

Cause: 
The PowerChute shutdown delay is set to high.

Solution:
Edit the pcnsconfig.ini file and change the shutdown command duration to 0 (zero) seconds.

Default configuration
[Shutdown]
shutdownCommand = 
shutdownCommandDuration = 60 

After the change
[Shutdown]
shutdownCommand = 
shutdownCommandDuration = 0