שאלות נפוצות
How can I have Vijeo Designer Runtime Windowed?
Issue:
How can I have Vijeo Designer Runtime Windowed?
Product Line:
Vijeo Designer, HMIG5U, HMIG5U2, HMIG5U21, HMIG5U22, Generic Windows PC
Resolution:
In order to view the Vijeo Designer Runtime windowed, please first disable "Windows Key Controls" in the property inspector (Setting will only be visible if the target type is Windows based) and then download to your HMI
Once the Windows Key Control is disabled, please hit "Control+Shift+V" and it will be windowed instead of full screen:
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
מוצר:
טווח:
גלה עוד
מוצר:
טווח: