undefined undefined
{}

המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
Do NetShelter™ Zero U Rack PDUs comes with vertical mounting brackets?
Issue:
Customers are asking if NetShelter™ Zero U Rack PDUs comes with vertical mounting brackets

Product Line:
NetShelter™ Zero U Rack PDUs

Environment:
NetShelter™ Rack PDU Advanced
NetShelter™ Metered Rack PDUs
NetShelter™ Switched Metered Outlet PDUs
NetShelter™ Switched Rack PDUs
NetShelter™ Metered-by-Outlet Rack PDUs

Solution:
NetShelter™ Zero U Rack PDUs do not come with vertical mounting brackets. They can be installed to the vertical accessory channel of a NetShelter™ rack using the included or pre-installed mounting pegs. The pegs will work in most rack enclosure designs. Please refer to the Installation Guide of your NetShelter™ Rack PDU for more info.
PDU Mounting PegsAPDU10K
For 3rd party cabinets, an alternative is utilizing the AR7711 (NetShelter Zero U Accessory Mounting Bracket).
AR7711

Kindly take note that this is specifically designed for NetShelter™ cabinets. We cannot guarantee fitment to 3rd party cabinets. It would be best to get in touch with the 3rd party manufacturer for options or compatibility concerns.

Should there be any further concerns, please contact our Customer Care Center at https://www.apc.com/us/en/support/

שניידר אלקטריק ישראל

גלה עוד
טווח:
מאמרים שעשויים להיות מועילים
גלה עוד
טווח: