undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the replacement of GSKC24VACDC.

Article available in these languages: Spanish

Emergency Stop function Preventa Safety module reference GSKC24VACDC  with 3 N/O S Safety Circuit
Outputs has been discontinued.Old reference GSKC24VACDC can be replaced by New Reference
XPSAK311144 Or XPS AF5130 based on customer application.
 
XPSAK311144 – Preventa Safety Module For Emergency stop, switch, sensing mat/edges or safety light curtain
monitoring with 3N/O safety circuit output and 1 N/C+ 4-solid-state signalling outputs for PLC, terminal block connection
integrated in module, supply voltage: 24VAC/DC.
 
XPSAF5130- Preventa Safety Module For Emergency stop and switch monitoring, with 3N/O safety circuit output,terminal
block connection integrated in module, supply voltage: 24VAC/DC.
 
Refer the attached file for technical catalogue of GSKC24VACDC, XPSAK311144 and XPSAF5130.

Schneider Electric India

Attachment(s)
Technical Catalogue_GSKC,XPSAK&XPSAF.zip [134.55 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more