{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is SIM mode and why it is required in DigitAN EM 6400 meter.
Simulation mode is provided for the purpose of demonstration of the features of the meter and in exhibition displays.
In this mode user can see the functioning of the meter without any input signals, meter shows fixed Frequency, voltage and
current and 0.5PF. Power and Energy parameters calculated based on this V (240VLN), A (5000A) and PF (-0.5) are displayed.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top