Search FAQs
How do we use G code file with SoMachine.
Refer to Somachine Project using G Code.
(CNC Application using Modicon LMC058 Controller).
(CNC Application using Modicon LMC058 Controller).
Short Description to use Program Example
1.The program has been made with SoMachine version V2.0RL1.
2.To use the program example,user need only a Modicon LMC058 Controller.
3.The Lexium 32A Servo Drives are configured in Virtual.
4.The procedure to use this example is:
Download the program to the LMC058 Controller.
Export the file "zzz.txt" to the LMC058 Controller.
With the visualization,start the function "SMC_ReadNCFile".
With the visualization, start the function "SMC_Interpolator".
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: