{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between Flywheel diodes surge suppressors and Bidirectional peak limiting diodes surge suppressors.
Flywheel Diode:-
The Flywheel diode surge suppressor is used to limit or remove the surges generated by the coil. Flywheel diode
 removes or limits the surge generated by the coil at the time of opening. With this surge suppressor the drop-out
time of coil increases up to 6- 10 times from the standard drop-out time of the coil.
 
Bidirectional peak limiting diode:-
The Bidirectional peak limiting diode surge suppressor provides the protection by limiting the transient voltage up
to 2Uc maximum. With this surge suppressor the opening time of coil remain as standard.
 

Schneider Electric India

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.