undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the difference between type 1 & type 2 SF circuit breaker.
The type 1 & type 2 SF circuit breaker has the below differences
 
- Poles are different (you can see upper insert T1 with one hole and T2 with two hole)
- Pressure of SF6 gas is different.
 
For SF1 Type 1: Means the pressure inside poles is 0,5 bar which means the capacity of SF CB if applicable for max. 630A.
 
For SF1 Type 2: The pressure is 2 bar which means the capacity of SF CB is max. 1250A.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.