Search FAQs
Can the Masterpact NW shunt trip and shunt close coils be remotely operated.
MX1-COM can be operated remotely by the circuit breaker communication module (BCM).
XF-COM can be operated remotely by the electrical close button (BPFE) or remotely by the circuit breaker
communication module (BCM).
communication module (BCM).
Select communicating coil MX/XF as per the supply voltage:-
Communicating Coil (1 part) | ||
AC 50/60 Hz DC | 12 Volts DC | 33032 |
24/30 Volts DC, 24 Volts AC | 33033 | |
48/60 Volts DC, 48 Volts AC | 33034 | |
100/130 Volts AC/DC | 33035 | |
200/250 Volts AC/DC | 33036 | |
277 Volts AC | 33037 | |
380/480 Volts AC | 33038 |
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: