Search FAQs
What is a Ground-Source return Ground Fault sensing system.
Ground-source return ground-fault sensing systems use one current sensor on the ground conductor connected to the circuit breaker
via a ground-fault interface module.
via a ground-fault interface module.
The current sensor measures the ground current flow.
The system location diagram below shows the current sensor in a three-phase, four-wire system. Ground-source return can also be used
on grounded systems which do not carry the neutral.
on grounded systems which do not carry the neutral.
Please refer the attached snapshot.
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: