Search FAQs
What are the functions of the Acti 9 Smart Test software
The main purpose of the Acti 9 Smart Test software is to help technical personnel to check that all devices are correctly
wired and function properly after installation.Acti 9 Smart Test software offers a quick test process based on a very intuitive
Graphical User Interface.
This software has the ability to deal with multiple Acti 9 Smartlink devices at the same time. They can be chained and only
one is connected to the computer. However, the fixed limit of connected Acti 9 Smartlink devices is 10.
wired and function properly after installation.Acti 9 Smart Test software offers a quick test process based on a very intuitive
Graphical User Interface.
This software has the ability to deal with multiple Acti 9 Smartlink devices at the same time. They can be chained and only
one is connected to the computer. However, the fixed limit of connected Acti 9 Smartlink devices is 10.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: