{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are categories of LV industrial switchgear, A and B, according to IEC 60947-2.
         There are two categories of LV industrial switchgear, A and B, according to IEC 60947-2
·         Those of category A, for which there is no deliberate delay in the operation of the “instantaneous” short-circuit magnetic
tripping device, are generally moulded-case type circuit-breakers, and

·         Those of category B for which, in order to discriminate with other circuit-breakers on a time basis, it is possible to delay
the tripping of the CB, where the fault-current level is lower than that of the short-time withstand current rating (Icw) of the.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top