Search FAQs
Can I transfer PLC application program from PC to PLC using Unity loader software.
The Unity Loader software provides the following transfer features:
- Transfer of a Unity Pro application from a PC to a Modicon M340, Premium or Quantum PLC.
- Transfer of a Unity Pro application from a Modicon M340, Premium or Quantum PLC to a PC.
- Transfer of firmware (FW) from a PC to a Modicon M340 PLC or to a module with firmware of the Modicon M340 platform.
Note: The Unity Loader software requires one of the following operating systems:
- Microsoft Windows XP Professional
- Microsoft Windows Vista Business
- Microsoft Windows 7 Professional
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: