Search FAQs
What is the Principle of Compensation by sector and its advantages in power factor correction system.
Principle of Compensation by Sector type Power Factor Correction:
Capacitor banks are connected to busbars of each local distribution board.
Advantages:
- Reduces the tariff penalties for excessive consumption of kvars
- Reduces the apparent power kVA demand, on which standing charges are usually based
- Relieves the supply transformer, which is then able to accept more load if necessary
- The size of the cables supplying the local distribution boards may be reduced, or will have additional capacity for possible load increases
- Losses in the same cables will be reduced
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: