{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to send command to control the digital output using Modbus protocol to PM5350.
For PM5350 meter, to energize Digital output, you should use command code 6003; to de-energize digital
output, you should use command code 6002.
 
Here is an example for writing register to "De-energize Digital Output DO2" via using Modbus tester (or PMC Modbus).
Select Data Type: W16 (to write Multiple registers);
Select Starting Register: 5250;
Select # of Resister: 3;
Write: 405250 ->6002; 405251 ->0; 405252->2
Press "Write" button.
 
Please keep in mind that the command write must be done in a block write and it will not work if you write each register individually!

Schneider Electric India

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.