Search FAQs
How to identify the Firmware version of EM6400/DM6200/PM1200.
There are 2 different methods to determine the firmware level in EM6400/DM6200/PM1200 meter if there is no
communications with the meter
1-The label on the back of the meter
2-From the front panel.
communications with the meter
1-The label on the back of the meter
2-From the front panel.
Refer the attached document for the procedure;
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: