The port numbers in the range from 0 to 1023 are the well-known ports. They are used by system processes that
provide widely used types of network services. The default ports are as below.
provide widely used types of network services. The default ports are as below.
FTP >> Port 21
HTTP >> Port 80
Modbus TCP >> 502
NTP >> 123
Telnet >> 23
Released for:Schneider Electric India
The port numbers in the range from 0 to 1023 are the well-known ports. They are used by system processes that
provide widely used types of network services. The default ports are as below.
provide widely used types of network services. The default ports are as below.
FTP >> Port 21
HTTP >> Port 80
Modbus TCP >> 502
NTP >> 123
Telnet >> 23
Released for:Schneider Electric India