undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the meaning of Err 7 in Altivar 58.
Err 7 is a Time out error, the display has sent a request to the control board and does not receive answer
It indicates a defect of communication between the display and the control board

Possible Root cause:
1 - Bad immunity (cable too long, bad earth connection ..)
2 - The baud rate of the RS485 serial link has been changed.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: