Search FAQs
How to do physical wiring of pulse output and contact rating of PM700P PowerLogic energy meter.
The physical wiring, as mentioned in the installation manual, there must be power source of 3 - 240 Vdc / 6 - 240 Vac with
no more than 100mA. Refer attached file for physical wiring.
no more than 100mA. Refer attached file for physical wiring.
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: