{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to setup PM820 relay output for under voltage alarm
To set up the own alarms for default KY digital output or even after installing an input/output module (PM8M2222) via display. For example, you may need to use
alarm under voltage to trigger output KY relay of PM820.
1). Go to MAINT/SETUP/Password=0/OK/ALARM/->/UNDER VAB/EDIT/+(ENABLE)/OK/+(MED)/OK/OK
2). Enter the maximum value PU mag=400/OK; pick-up delay PU delay=1/OK; drop-out value DO Mag=390/OK; drop-out delay DO delay=1/OK
3). Press up button and select "YES" to save the change.
4). Go to MAINT>SETUP>I/O>D OUT (digital out)-->KY /EDIT/NORM/OK/change EXT. to ALARM
5). Press to select alarm type: UNDER VAB, to active the alarm, press + until asterisks appears like: ** AL-XX**
6). Press up button and select "YES" to save the change. In this way customer is able to customize their own alarm. The contact is as NO mode.

Schneider Electric India