{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How can we check the cable fault from Sepam MET148-2 module for temperature sensor inputs to Motor sensor (PT 100 or Ni 100).
The temperature monitoring function provided by Sepam T81, T82, T87, M81, M87, M88, G82, G87, G88, C86 units checks the connection of each RTD that is configured.
An "RTD FAULT" alarm is generated whenever one of the RTDs is detected as being short-circuited or disconnected (absent).
To identify the faulty RTD or RTDs:
1. Display the temperature values measured by Sepam using the SFT2841 software.
2. Check the consistency of the temperatures measured:
a. the temperature displayed is "****" if the RTD is short-circuited (T < -35 °C or T < -31° F).
b. the temperature displayed is "-****" if the RTD is disconnected (T > 205 °C or T > 401° F).

Schneider Electric India

How can we check the cable fault from Sepam MET148-2 module for temperature sensor inputs to Motor sensor (PT 100 or Ni 100).
The temperature monitoring function provided by Sepam T81, T82, T87, M81, M87, M88, G82, G87, G88, C86 units checks the connection of each RTD that is configured. 
An "RTD FAULT" alarm is generated whenever one of the RTDs is detected as being short-circuited or disconnected (absent). 
To identify the faulty RTD or RTDs: 
1. Display the temperature values measured by Sepam using the SFT2841 software. 
2. Check the consistency of the temperatures measured: 
a. the temperature displayed is "****" if the RTD is short-circuited (T < -35 °C or T < -31° F).
b. the temperature displayed is "-****" if the RTD is disconnected (T > 205 °C or T > 401° F). 
 

Schneider Electric India
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
Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top