{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the Modbus register addresses of the Zelio Logic communications module SR3MBU01BD?
The SR3MBU01BD is a communication module for  the Zelio Smart Relay SR3 (24Vdc) that allows the Zelio to be used in a Modbus Serial Network:

image1
Zelio SR3 will be slave in the network so a Master is needed.

The input register addresses are %MW16 - %MW19 but are only available in FBD, not Ladder.
The output register addresses are %MW20 - %MW23.
The Zelio clock can be interrogated using registers %MW32 - %MW35.

The attached file gives more detailed information.

If you need a Master in the Modbus Serial network then the best solution will be to use a PLC like the Modicon M221.
For further information about the complete range of PLCs check our Digital catalog:
https://digicat.se.com/

Schneider Electric India

Attachment(s)
SR3 MRU01.pdf [774.26 KB]