{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Troubleshooting tips if Power Meter PM710 can not communicate on RS485 modbus network.

Refer below troubleshooting tips if power meter can not communicate from a remote personal computer or modbus client software.

Casue1: Power meter address is incorrect.
Solution : Check to see that the power meter is correctly addressed.

Casue2: Power meter baud rate (parity, stop bit) is incorrect.
Solution: Verify that the baud rate of the power meter matches the baud rate of all other devices on its communications link.

Cause3: Communications lines are improperly connected.
Solution: Verify the power meter communications connections.

Cause4: Communications lines are improperly terminated.
Solution: Check to see that a multipoint communications terminator is properly installed.

Schneider Electric India

Explore more
Range:
PowerLogic PM700 series
Explore more
Range:
PowerLogic PM700 series
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.