Search FAQs
What are the Acti9 range meter models with pulse output are compatible with the Acti9 Smartlink
Schneider Electric energy meters as per the below listed references with pulse output are compatible with the Acti 9 Smartlink;
****** Direct measurement (up to 63 A)
1. iEM3110 (the pulse weight can be configured)
2. iEM3155 (the pulse weight can be configured)
*****CTs inputs (1 A, 5A)
3. iEM3210 (the pulse weight can be configured)
4. iEM3255 (the pulse weight can be configured)
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: