Search FAQs
What are the technical details of DK1JC23 and what is the standard cross reference of DK1-JC23 reference
The DK1JC23 was a 3 poles fuses switch disconnector size 1 fuse rated for 315A maximum. Please refer the attached available catalog page for the technical specification of DK1JC23
Today it can be replace by GS2QQ* fuse switch disconnector range from available offer. You will have to be aware the the fuse in GS2QQ will size 2.
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: