undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the dv/dt value at Motor terminals with the Motor choke using Altivar 71/61 drive.
Motor chokes allow to limit the dv/dt at the motor terminals to:

>> 500 V/us for 200…400 V and 380…480 V three-phase line supplies.

>> 1000 V/us for 500…690 V three-phase line supplies.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: