Search FAQs
While communicating Altivar 212 drive in RJ45 modbus communication with SoMove lite software & nbsp, it shows & quot;Attention - Local forcing appeared & quot; when connecting & disconnecting. what could be the possible reasons & nbsp;
Message "Local Forcing appeared" is pop up on screen of SoMoveLite to indicate that ATV212 drive's Local mode.
![Local_Forcing_image](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000CluHuQAJ&oid=00DA0000000abSmMAI)
This message can only be seen on screen of SoMoveLite while Connecting or Disconnecting the drives under the following two conditions
1.
Drive Local Mode is ON. one have pressed LOC/ REM button of local display and hence drive is in local mode. If during this time, one try to connect or disconnect drive then message "Local Forcing appeared" can be seen and it is obvious.
2.
If "Forced Local Mode" is activated. This can be activated through one of the logic input F, R or RES by assigning 48 to any of the programmable logic inputs. When respective logic input which is assigned with value 48 (Forced Local Mode) and if that particular Logic input is ON at that time drive is in Forced Local Mode. If during this time, you try to connect or disconnect drive then message "Local Forcing appeared" can be seen and it is obvious.
Note: This is note a kind of error or alarm message but it is an indication to user only.
This message can only be seen on screen of SoMoveLite while Connecting or Disconnecting the drives under the following two conditions
1.
Drive Local Mode is ON. one have pressed LOC/ REM button of local display and hence drive is in local mode. If during this time, one try to connect or disconnect drive then message "Local Forcing appeared" can be seen and it is obvious.
2.
If "Forced Local Mode" is activated. This can be activated through one of the logic input F, R or RES by assigning 48 to any of the programmable logic inputs. When respective logic input which is assigned with value 48 (Forced Local Mode) and if that particular Logic input is ON at that time drive is in Forced Local Mode. If during this time, you try to connect or disconnect drive then message "Local Forcing appeared" can be seen and it is obvious.
Note: This is note a kind of error or alarm message but it is an indication to user only.
Released for:Schneider Electric India
Explore more
Range:
Product:
Explore more
Range:
Product: